AXIS#.SAFE.SBC.ACTIVE

Description

Indicates whether Safe Brake Control (SBC) is active or not. When SBC is active the brake cannot be commanded to release. If SBC is enabled, it is executed once stopped during all stopping safety functions. Once the safety function condition clears, SBC will stop and allow the brake to be released.

Context

For complete SBC information refer to SBC (Safe Brake Control).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read Only

Units

N/A

Range

0 or 1
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
AXIS1.SAFE.SBC.ACTIVE

2061h

00h

Unsigned8

-

-

Read only

Yes

AXIS2.SAFE.SBC.ACTIVE

2161h

00h

Unsigned8

-

-

Read only

Yes